20.3.3 Advanced Analysis of I/Os
SmartPower provides an easy way of estimating the power consumption related to I/Os. You can then analyze power consumption in detail.
To display I/O power consumption:
- In the Summary tab, select By Type from the
Breakdown drop-down list. The grid displays the total
power consumption of all I/Os in the design, as well as all other components. If you
use different I/O standards, and
different Vcci power rails, you can also display the power consumption for each rail by selecting By Rail from the Breakdown drop-down list. Breakdown By Rail shows the power consumption and current for each Vcci rail in the design.
-
- In the Analysis tab, select the highest hierarchy level in
the Hierarchy tree in the left pane. Select By
Instance from the Breakdown drop-down list.
- In the Analysis tab, unselect all categories under Instances Contributions except I/Os, and then click Apply. The table then displays a list of all I/Os in the design, along with the power contribution of each individual I/O. The columns display important I/O attributes: external port name, load, standard, drive-strength, slew, and macro.
- In the Probabilities tab, you can control the output probability of each tri-state and bidirectional I/O. The probability is the percentage of time that the I/O is used as an output. The default value can be changed and a specific value can also be set for each bidirectional or tri-state I/O.
- In the Analysis tab, select the highest hierarchy level in
the Hierarchy tree in the left pane. Select By
Instance from the Breakdown drop-down list.