5.33.3.2 Procedures created with the proc command
You use the proc command to declare a procedure. You can then use the name of the procedure as a Tcl command. The following sample script consists of a single command named proc. The proc command takes three arguments:
- The name of a procedure (myproc)
- A list of argument names (arg1 arg2)
- The body of the procedure, which is a Tcl script
proc myproc { arg1 arg2 } { # procedure body
}
myproc a b