8.8.2 Structural Simulation
Use the following procedures to perform a structural simulation of an Actel design. Refer to the Innoveda documentation for additional information about performing simulation with SpeedWave.
- Synthesize your design. Refer to the documentation included with your synthesis tool for information about synthesis.
- Select your Actel project in Project Manager. If you have not created your project, go to Project Setup for the procedure.
- Open the HDL Manager. This displays the HDL manager dialog box.
- Open a project HDL workspace (.hws) file. Choose the Open command from the File menu. Select an .hws file and click the Open button in the Open dialog box.
- Analyze your structural VHDL netlist
and testbench. If you have not already generated a structural VHDL netlist, go to
Generating a Structural VHDL Netlist for the procedure. Select the user
library icon in the VHDL User Libraries section of the VHDL View window. Choose the
Add Source Files command from the Library menu. The Assign Source Files dialog box
is displayed. Select the structural VHDL netlist and testbench files from the VHDL
Source File Name window and click OK. Select each file and
choose the Analyze Source File command from the Analyze menu. Check the Output
window for successful completion. Save the HDL workspace and close the HDL Manager
window.Note: SpeedWave can only simulate configurations. You must have at least one configuration in your testbench.
- Select a configuration to simulate. Choose the Load
Design command from the File menu.
Double-click
user.liband select the configuration you want to simulate. Click OK. A Source Viewer window and a Hierarchy Viewer window are displayed. - Simulate your design. Choose the Run Simulation command from the Simulate menu. The Run Simulation dialog box is displayed. Select the desired options and click the Apply button. Click the Close button when you have completed your simulation.