15.11.5 Editing Active Lists
You can change the name of an existing active list as well as modify its contents.
To edit an Active List:
- Select the active list to edit.
- From the View menu, choose Edit Current Active List.
The Edit Active List dialog box appears with the properties of the selected active list.
- In the Edit Active List dialog box, modify the properties you want to change.
- Click OK.