15.11.4 Copying Active Lists
You can copy and modify existing active lists. This feature is useful if you want to create a new list that is similar to but not exactly the same as an existing active list.
To copy an Active List:
- From either the Tools or View menu, choose Active Lists > More Active Lists.
- In the More Active Lists dialog box, select the list to copy, and click Copy.
- In the Save List Copy As dialog box, enter a name for your new active list. This list will contain the same properties as the one being copied.
- Click OK. Your new list now appears in the More Active Lists dialog box.
- Click Edit to display the Edit Active Lists dialog box in which you can modify the properties of the list.
- Click OK to save your changes.
- Click Close to close the More Active Lists dialog box.
The newly created active list now appears on both the Tools and View menus.