5.6.7 Source Files for Simulation
The Source Files for Simulation dialog box enables you to set the simulation file order in the Project Manager.
De-select the Use default list from Project Manager checkbox to Add/Remove source files for simulation.
To specify the simulation file order:
- From the Project menu, choose . The Organize Source Files for Simulation dialog box appears.
- De-select the Use default list from Project Manager checkbox to Add/Remove source files for simulation. Click the Default button to reset the options to the original settings.
- Click OK.