13.32.18.2 Wildcard Characters
You can use the following wildcard characters in names used in Tcl commands:
| Wildcard | What it Does |
|---|---|
|
\ |
Interprets the next character literally |
|
? |
Matches any single character |
|
* |
Matches any string |
|
[] |
Matches any single character among those listed between brackets (that is, [A-Z] matches any single character in the A-to-Z range) |
Note: The matching function requires that you add a slash (\) before each slash in the port,
instance, or net name when using wildcards in a PDC command and when using wildcards in the
Find feature of the MultiView Navigator. For example, if you have an instance named “A/B12”
in the netlist, and you enter that name as “A\\/B*” in a PDC command, you will not be able
to find it. In this case, you must specify the name as A\\\\/B*.