5.33.8.4 catch statement
A "catch" statement suspends normal error handling on the enclosed Tcl command. If a variable name is also used, then the return value of the enclosed Tcl command is stored in the variable.
catch { open “$inputFile” r } myresult