13.2.3 Opening your Libero IDE Project
The Project Manager opens your most recent project automatically. You can change your default startup preferences in the Startup tab.
To open a different project in Project Manager:
- From the File menu, choose Close Project.
- From the File menu, choose Open Project or New Project. If you create a new project the Project Manager starts the New Project Wizard.
Note: The last five saved projects are available from the File menu. From the File
menu, choose Recent Projects, and then select the project to open.
You can open an existing project by double-clicking the *.prj file or dragging
the *.prj file over the Libero IDE desktop icon.