1.2.5.5 WDRV_PIC32MZW_BSSCtxIsValid Function
bool WDRV_PIC32MZW_BSSCtxIsValid (
const WDRV_PIC32MZW_BSS_CONTEXT *const pBSSCtx, bool ssidValid
)
C
Summary
Tests if a BSS context is valid.
Description
Tests the elements of the BSS context to judge if their values are legal.
Precondition
None.
Parameters
Param | Description |
pBSSCtx | Pointer to a BSS context. |
ssidValid | Flag indicating if the SSID within the context must be valid. |
Returns
true or false indicating if context is valid.
Remarks
A valid SSID is one which has a non-zero length. The check is optional as it is legal for the SSID field to be zero length.