1.2.5.10 WDRV_PIC32MZW_BSSCtxSetSSIDVisibility Function
WDRV_PIC32MZW_STATUS WDRV_PIC32MZW_BSSCtxSetSSIDVisibility (
WDRV_PIC32MZW_BSS_CONTEXT *const pBSSCtx, bool visible
)
C
Summary
Configures the visibility of the BSS context.
Description
Specific to Soft-AP mode this flag defines if the BSS context will create a visible presence on air.
Precondition
None.
Parameters
Param | Description |
pBSSCtx | Pointer to a BSS context. |
visible | Flag indicating if this BSS will be visible or not. |
Returns
WDRV_PIC32MZW_STATUS_OK - The context has been configured. WDRV_PIC32MZW_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_PIC32MZW_STATUS_INVALID_CONTEXT - The BSS context is not valid.
Remarks
None.
Client Interface - Authentication Context APIs
The authentication context contains information relevant to the authentication mechanisms used in Wi-Fi. Currently supported are Open, WPA/WPA2/WPA3-Personal and WPA/WPA2/WPA3- Enterprise(EAP-TLS). . The structure WDRV_PIC32MZW_AUTH_CONTEXT is provided to contain the
context. To initialize a context, the function WDRV_PIC32MZW_AuthCtxSetDefaults is provided, which ensures the context is in a known state. The function WDRV_PIC32MZW_AuthCtxIsValid is provided to test if a context is valid. Each authentication type has at least one function which can be used to configure the type of authentication algorithm used as well as the parameters which are required.