1.14 CRYPT_AES_DIRECT_Decrypt Function

C

int CRYPT_AES_DIRECT_Decrypt(
    CRYPT_AES_CTX* aes,
    unsigned char* out,
    const unsigned char* in
);

Description

This function decrypts one block of data, equal to the AES block size.

Preconditions

Key and Initialization Vector (IV) must be set earlier with a call to CRYPT_AES_KeySet and CRYPT_AES_IvSet.

Parameters

ParametersDescription
aesPointer to context which saves state between calls
outPointer to buffer to store the results of the decryption
inPointer to buffer where the data to decrypt is located

Returns

  • BAD_FUNC_ARG - An invalid pointer was passed to the function
  • 0 - An invalid pointer was not passed to the function

Remarks

Input and output buffers must be equal in size (CRYPT_AES_BLOCK_SIZE).

Example

CRYPT_AES_CTX mcAes;
int           ret;
byte          out1[CRYPT_AES_BLOCK_SIZE];
byte          out2[CRYPT_AES_BLOCK_SIZE];

strncpy((char*)key, "1234567890abcdefghijklmnopqrstuv", 32);
strncpy((char*)iv,  "1234567890abcdef", 16);

ret = CRYPT_AES_KeySet(&mcAes, key, 16, iv, CRYPT_AES_ENCRYPTION);
ret = CRYPT_AES_DIRECT_Decrypt(&mcAes, out2, out1);