1.55 CRYPT_SHA224_DataAdd Function

C

int CRYPT_SHA224_DataAdd(
    CRYPT_SHA256_CTX* sha224,
    const unsigned char* input,
    unsigned int sz
);

Description

This function updates the hash with the data provided.

Preconditions

The SHA224 context must be initialized prior to the first call of this function. The context must not be modified by code outside of this function.

Parameters

ParametersDescription
sha224Pointer to CRYPT_SHA256_CTX structure which holds the hash values
inputPointer to the data to use to update the hash
szSize of the data (in bytes) to use to update the hash

Returns

  • BAD_FUNC_ARG - An invalid pointer was passed to the function, either in sha224 or input
  • 0 - An invalid pointer was not passed to the function

Remarks

In order to preserve the validity of the SHA224 hash, nothing must modify the context holding variable between calls to CRYPT_SHA224_DataAdd.

Example

CRYPT_SHA256_CTX sha224;
uint8_t buffer[1024];
uint8_t shaSum[SHA224_DIGEST_SIZE];

CRYPT_SHA224_Initialize(&sha224);
CRYPT_SHA224_DataAdd(&sha224, buffer, sizeof(buffer));
CRYPT_SHA224_Finalize(&sha224, shaSum);