1.70 CRYPT_SHA512_Initialize Function
C
int CRYPT_SHA512_Initialize(
CRYPT_SHA512_CTX* sha512
);Description
This function initializes the internal structures necessary for SHA512 hash calculations.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| sha512 | Pointer to CRYPT_SHA512_CTX structure which holds the hash values |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- 0 - An invalid pointer was not passed to the function
Remarks
All SHA512 hashes have to start at a particular value before adding new data to it. This function sets the necessary values for the structure.
Example
CRYPT_SHA512_CTX sha512; uint8_t sha512Sum[SHA512_DIGEST_SIZE]; CRYPT_SHA512_Initialize(&sha512); CRYPT_SHA512_DataAdd(&sha512, buffer, sizeof(buffer)); CRYPT_SHA512_Finalize(&sha512, sha512Sum);