1.36 CRYPT_RSA_Initialize Function
C
int CRYPT_RSA_Initialize(
CRYPT_RSA_CTX* rsa
);Description
This function initializes the context used during public-key RSA encryption and decryption.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to RSA context which saves state between calls |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- -1 - Unable to allocate the memory necessary for the key
- 0 - An invalid pointer was not passed to the function
Example
CRYPT_RSA_CTX mcRsa; int ret; ret = CRYPT_RSA_Initialize(&mcRsa);