1.12 CRYPT_AES_CTR_Encrypt Function
C
int CRYPT_AES_CTR_Encrypt(
CRYPT_AES_CTX* aes,
unsigned char* out,
const unsigned char* in,
unsigned int inSz
);Description
This function encrypts a block of data using the AES algorithm in Counter (CTR) mode.
Preconditions
Key and Initialization Vector (IV) must be set earlier with a call to CRYPT_AES_KeySet and CRYPT_AES_IvSet.
Parameters
| Parameters | Description |
|---|---|
| aes | Pointer to context which saves state between calls |
| out | Pointer to buffer to store the results of the encryption pass |
| in | Pointer to buffer holding the data to be encrypted |
| inSz | Size of the input data, in bytes |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- 0 - An invalid pointer was not passed to the function
Remarks
The output buffer must be equal in size to the input buffer.
Example
CRYPT_AES_CTX mcAes; int ret; byte out1[AES_TEST_SIZE]; strncpy((char*)key, "1234567890abcdefghijklmnopqrstuv", 32); strncpy((char*)iv, "1234567890abcdef", 16); ret = CRYPT_AES_KeySet(&mcAes, key, 16, iv, CRYPT_AES_ENCRYPTION); ret = CRYPT_AES_CTR_Encrypt(&mcAes, out1, ourData, AES_TEST_SIZE);