1.38 CRYPT_RSA_PrivateKeyDecode Function
C
int CRYPT_RSA_PrivateKeyDecode(
CRYPT_RSA_CTX* rsa,
const unsigned char* in,
unsigned int inSz
);Description
This function builds a private key from a DER-formatted certificate. DER stands for Distinguished Encoding Rules.
Preconditions
The context must have been initialized with a call to CRYPT_RSA_Initialize.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context which saves state between calls |
| in | Pointer to buffer containing the certificate to process to extract the private key |
| inSz | Size of the input data in bytes |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- 0 - An invalid pointer was not passed to the function
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa; int ret; unsigned int keySz = (unsigned int)sizeof(client_key_der_1024); ret = CRYPT_RSA_Initialize(&mcRsa); ret = CRYPT_RSA_PrivateKeyDecode(&mcRsa, client_key_der_1024, keySz);