1.35 CRYPT_RSA_Free Function
C
int CRYPT_RSA_Free(
CRYPT_RSA_CTX* rsa
);Description
This function releases the memory used during RSA processing for storing the public/private key.
Preconditions
The context must have been set up previously with a call to CRYPT_RSA_Initialize.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context to clean up |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- 0 - An invalid pointer was not passed to the function
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa; int ret; ret = CRYPT_RSA_Initialize(&mcRsa); ret = CRYPT_RSA_Free(&mcRsa);