1.32 CRYPT_ECC_SignatureSizeGet Function
C
int CRYPT_ECC_SignatureSizeGet(
CRYPT_ECC_CTX* ecc
);Description
This function returns the size of the signature in a given context, in octets.
Preconditions
The ECC context must have been initialized with a call to CRYPT_ECC_Initialize. The keys must have been imported or created prior to calling this function.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls, and contains the signature |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- int - The size of the signature
Remarks
None.
Example
CRYPT_ECC_CTX userA; int ret; byte sig[100]; unsigned int sigSz = (unsigned int)sizeof(sig); unsigned int usedA = 0; ret = CRYPT_ECC_Initialize(&userA); ... // Import or generate private key ... ret = CRYPT_ECC_SignatureSizeGet(&userA);