1.16 CRYPT_AES_GCM_Decrypt Function

C

int CRYPT_AES_GCM_Decrypt(
    CRYPT_AES_CTX* aes,
    unsigned char* out,
    const unsigned char* in,
    unsigned int sz,
    const unsigned char* iv,
    unsigned int ivSz,
    const unsigned char* authTag,
    unsigned int authTagSz,
    const unsigned char* authIn,
    unsigned int authInSz
);

Description

This function decrypts a block of data using the AES algorithm in Galois/Counter Mode (GCM).

Preconditions

Key must be set earlier with a call to CRYPT_AES_GCM_SetKey.

Parameters

ParametersDescription
aesPointer to context which saves state between calls
outPointer to buffer to store the results of the decryption pass
inPointer to buffer holding the data to be decrypted
szSize of the input data, in bytes
ivPointer to the initialization vector
ivSzSize of the initialization vector
authTagPointer to the buffer to store the authentication tag
authTagSzSize of the authentication tag
authInPointer to the additional authentication data
authInSzSize of the additional authentication data

Returns

  • BAD_FUNC_ARG - An invalid pointer was passed to the function
  • AES_GCM_AUTH_E - The authTag is incorrect
  • 0 - An invalid pointer was not passed to the function

Remarks

The output buffer must be equal in size to the input buffer.