1.30 CRYPT_ECC_PublicExport Function
C
int CRYPT_ECC_PublicExport(
CRYPT_ECC_CTX* ecc,
unsigned char* out,
unsigned int outSz,
unsigned int* usedSz
);Description
This function takes an ECC public key and exports it in ANSI X9.63 format.
Preconditions
The context must be initialized previously with a call to CRYPT_ECC_Initialize. The key must also have been constructed with a call to CRYPT_ECC_DHE_KeyMake. A random number generator must have been initialized with a call to CRYPT_RNG_Initialize.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls |
| out | Buffer in which to store the public key |
| outSz | The available size of the buffer, in bytes |
| usedSz | Return value indicating how many bytes were used |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- BUFFER_E - The output buffer was too small to store the key
- 0 - An invalid pointer was not passed to the function
Remarks
None.
Example
CRYPT_ECC_CTX userA; int ret; byte sharedA[100]; unsigned int aSz = (unsigned int)sizeof(sharedA); unsigned int usedA = 0; ret = CRYPT_ECC_Initialize(&userA); ret = CRYPT_ECC_DHE_KeyMake(&userA, &mcRng, 32); ret = CRYPT_ECC_PublicExport(&userA, sharedA, aSz, &usedA);