1.28 CRYPT_ECC_KeySizeGet Function
C
int CRYPT_ECC_KeySizeGet(
CRYPT_ECC_CTX* ecc
);Description
This function returns the size of the ECC key, in octets.
Preconditions
The ECC context must have been initialized with a call to CRYPT_ECC_Initialize. The key must have been imported or created prior to calling this function.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls and contains the key |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function
- int - The size of the key, in octets
Remarks
None.
Example
CRYPT_ECC_CTX userA; int ret; byte sig[100]; unsigned int sigSz = (unsigned int)sizeof(sig); unsigned int usedA = 0; ret = CRYPT_ECC_Initialize(&userA); ... // Import or generate private key ... ret = CRYPT_ECC_KeySizeGet(&userA);