1.26 CRYPT_ECC_Free Function

C

int CRYPT_ECC_Free(
    CRYPT_ECC_CTX* ecc
);

Description

This function cleans up memory allocated for an ECC Context.

Preconditions

The context must have been initialized previously with a call to CRYPT_ECC_Initialize.

Parameters

ParametersDescription
eccPointer to context to clean up

Returns

  • BAD_FUNC_ARG - An invalid pointer was passed to the function
  • 0 - An invalid pointer was not passed to the function

Remarks

None.

Example

CRYPT_ECC_CTX userA;
int           ret;

ret = CRYPT_ECC_Initialize(&userA);
...
ret = CRYPT_ECC_Free(&userA);