1.69 CRYPT_SHA512_Finalize Function

C

int CRYPT_SHA512_Finalize(
    CRYPT_SHA512_CTX* sha512,
    unsigned char* digest
);

Description

This function finalizes the hash and puts the result into digest.

Preconditions

The SHA512 context must be initialized prior to calling this function. The context must not be modified by code outside of this function.

Parameters

ParametersDescription
sha512Pointer to CRYPT_SHA512_CTX structure which holds the hash values
digestPointer to byte array to store hash result

Returns

  • BAD_FUNC_ARG - An invalid pointer was passed to the function, either in sha512 or digest
  • 0 - An invalid pointer was not passed to the function

Remarks

In order to preserve the validity of the SHA512 hash, nothing must modify the context holding variable between calls to CRYPT_SHA512_DataAdd and CRYPT_SHA512_Finalize.

Example

CRYPT_SHA512_CTX sha512;
uint8_t buffer[1024];
uint8_t sha512Sum[SHA512_DIGEST_SIZE];

CRYPT_SHA512_Initialize(&sha512);
CRYPT_SHA512_DataAdd(&sha512, buffer, sizeof(buffer));
CRYPT_SHA512_Finalize(&sha512, sha512Sum);