3.4.1 PKOB4 and MCP2200

PKOB4 and MCP2200 USB devices are accessible to the upstream PC via a common USB connector (J100) using the Microchip USB 2.0 High Speed Hub Controller USB2512B providing the user with more ease of use.

After plugging the PIC32-BZ6 Curiosity Board into the upstream PC using a USB cable, device enumeration is as illustrated in the following figure for the PKOB4 and MCP2200.
Figure 3-4. Device Manager