9.3.24 Input Delay

Sets the Input Delay.

Input Delay applies to all I/O standards. The range of values supported varies depending on the device selected. The default value is OFF.

Note: This attribute will not appear in the I/O attributes and cannot be used in the PDC for some I/Os with dynamic delays, such as DDR I/Os.