9.3.31 Output Delay

Sets the Output Delay.

Output Delay applies to all I/O standards. The range of values supported varies depending on the device selected. The default value is OFF. The default value is OFF.

Direction: Output

Note: This attribute will not appear in the I/O attributes and cannot be used in the PDC for some I/Os with dynamic delays, such as DDR I/Os.