21.10.15 set_manufacturer
(Ask a Question)Description
This command specifies the manufacturer for the SPI Flash device.
set_manufacturer {MICRON | SPANSION | Macronix | Winbond }
Arguments
Parameter | Type | Description |
---|---|---|
None | string | The value for the set_manufacturer command must be one of the following:
|
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | None |
Supported Families
PolarFire® |
PolarFire SoC |
Example
This example sets the manufacturer {MICRON}.
set_manufacturer {MICRON}