Description
This Tcl command appears in the fabric RAM configuration file when the Fabric RAM is
modified to initialize memory.
modified_client \
-logical_instance_name { RAM user defined instance name } \
-storage_type { Initialization client storage type } \
-content_type { NO_CONTENT | MEMORY_FILE } \
-memory_file_format { Intel-Hex | Motorola-S | Simple-Hex | Microsemi-Binary } \
-memory_file { path }
Arguments
Parameter | Type | Description |
logical_instance_name |
string |
Specifies the name of the user defined memory instance. |
storage_type |
string |
Specifies storage type to initialize RAM: |
content_type |
string |
Specifies the type of memory content:
- MEMORY_FILE -
content_file parameter must be specified.
- NO_CONTENT -
no content memory file.
|
memory_file_format |
string |
Specifies the memory file format:
- Intel-Hex
- Motorola-S
- Simple-Hex
- Microchip-Binary
|
memory_file |
string |
Specifies the absolute or relative path of the memory
file. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | None |
Example
The following example show the modified_client
Tcl command.
modified_client \
-logical_instance_name {PF_TPSRAM_C0_0/PF_TPSRAM_C0_0} \
-storage_type {SNVM} \
-content_type {MEMORY_FILE} \
-memory_file_format {Intel-Hex} \
-memory_file {Y:/TP_mem/TPRAM_1024_40lp/mem_files/hex .hex}