3.5.1.24.1 Background: LLVM Internal Representation used by SmartHLS™
(Ask a Question)The instructions displayed in the Schedule Viewer are from the LLVM compiler that SmartHLS is built on. These assembly-like instructions are called LLVM intermediate representation (IR) . Some understanding of the LLVM IR is beneficial when using the Schedule Viewer.
For example, given the 32-bit code:
result = a + b - 5
This C++ code could be represented as instructions in LLVM IR as:
%0 = add i32 %a, %b %result = sub i32 %0, 5
In LLVM IR, intermediate variables are prefixed with a “%”. Each operation (add/sub) includes the bitwidth “i32” indicating 32-bit integer. The add operands are %a + %b and the result is stored in a temporary 32-bit variable %0. The subtract operands are %0 – 5 and the result is stored in the variable %result.
Basic blocks are also important concepts in LLVM IR. A basic block is a group of instructions that always run together with a single entry point at the beginning and a single exit point at the end. A basic block in LLVM IR always has a label at the beginning and a branching instruction at the end (br
, ret
, etc.). Control flow occurs between basic blocks.
Here the body.0
basic block performs some operations and then branches unconditionally to another basic block labeled body.1
.
body.0: %0 = add i32 %a, %b %result = sub i32 %0, 5 br label %body.1
All of the basic blocks and instructions shown in the Scheduler Viewer are directly from the LLVM IR optimized by SmartHLS before being compiled into Verilog.