3.5.1.26.3 Control Flow Graph
(Ask a Question)The Control Flow Graph can be brought up by clicking on any function in the Explorer tab. The Control Flow Graph shows the connections between basic blocks and shows which basic blocks can branch to which other basic blocks. Each basic block in graph is showed with the corresponding source location consists of the filename and line numbers. The cycle latency of the basic block is also showed in the graph.
For example the following code has an if/else statement and then a for-loop in the else body. This has multiple code blocks and branches to different sections of the code.
volatile int gv = 1; #define N 1000 int main() { if (gv) { return 0; } else { for (int i = 0; i < N; i++) { gv++; } return 0; } }
This Control Flow Graph shows the two paths of the if statement on the right and the else statement on the left, and the for-loop in the left middle bubbles. Control flow is represented by an arrow, where a basic block will only branch into another basic block that it points to.