Description
Disables
timing arcs within a cell
(instance) and returns the ID of the created constraint if the
command succeeded. To specify a Disable Timing constraint, open the Set Constraint
to Disable Timing Arcs dialog box in the following way:
From
the
Constraints
menu,
click
Disable Timing.
Note: This constraint is for the
Place and Route tool and the Verify Timing tool. It is ignored by the Synthesis
tool.
set_disable_timing -from value -to value name
Arguments
| Parameter | Type | Description |
|---|
from | string | Specifies the starting point for the timing arc. The -from and -to arguments must either both be present or both omitted for the constraint to be valid. |
to | string | Specifies the ending point for the timing arc. The -from and -to arguments must either both be present or both omitted for the constraint to be valid. |
name | string | Specifies the instance(cell) name for which the disable timing arc constraint will be created. |
| Return Type | Description |
|---|
integer | Returns the ID of created constraint. |
Error Codes
| Error Code | Description |
|---|
| None | Required parameter _AtclParam0_ is missing. |
Supported
Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Example
The following example disables timing arcs within A to Y.
set_disable_timing -from A -to Y
Related Examples on GitHub