21.8.40 remove_generated_clock
(Ask a Question)Description
Removes the specified generated clock constraint from the current scenario. If the specified name does not match a generated clock constraint in the current scenario, or if the specified ID does not refer to a generated clock constraint, this command fails.
Do not specify both the clock and port names and the constraint ID.
remove_generated_clock -name clock_name | -id constraint_IDArguments
| Parameter | Type | Description |
|---|---|---|
name | string | Specifies the name of the generated clock constraint to remove from the current scenario. You must specify either a clock name or an ID. |
id | integer | Specifies the ID of the generated clock constraint to remove from the current scenario. You must specify either an ID or a clock name that exists in the current scenario. |
Error Codes
| Error Code | Description |
|---|---|
| None | Invalid clock name argument. |
| None | Only one argument is needed. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Exceptions
You cannot use wildcards when specifying a clock name.
Example
The following example removes the generated clock constraint named
my_user_clock
remove_generated_clock -name my_user_clock