21.8.8 create_scenario
(Ask a Question)Description
Creates a new timing scenario with the specified name. You must provide a unique name (that is, it cannot already be used by another timing scenario).
A timing scenario is a set of timing constraints used with a design. Scenarios enable you to easily refine the set of timing constraints used for Timing-Driven Place-and-Route, so as to achieve timing closure more rapidly.
This command creates an empty timing scenario with the specified name and adds it to the list of scenarios.
Note: It is recommended to use the
organize_tool_files command instead of this command.create_scenario nameArguments
| Parameter | Type | Description |
|---|---|---|
name | string | Specifies the name of the new timing scenario. This is mandatory. |
Error Codes
| Error Code | Description |
|---|---|
| None | Required parameter _AtclParam0_ is missing. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Example
The following example creates a new timing scenario with the "scenario_A" name.
create_scenario scenario_A