Description
Returns
the details for all the existing clock groups in the current timing constraint
scenario.
list_clock_groups
Arguments
| Parameter | Type | Description |
|---|
None | None | None |
| Return Type | Description |
|---|
string | Details about all of the clock groups constraints in the current timing constraint scenario. |
Supported
Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Example
With this command we get the details about all of the existing clock groups in the current timing constraint scenario.
puts [list_clock_groups]
Related Examples on GitHub