21.8.47 remove_set
(Ask a Question)Description
Removes a set of paths from analysis. Only user-created sets can be deleted.
remove_set -name nameArguments
| Parameter | Type | Description |
|---|---|---|
name | string | Specifies the name of the set of paths to delete. |
Error Codes
| Error Code | Description |
|---|---|
| None | Required parameter -name is missing. |
| None | Unable to find set. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Exceptions
You cannot use wildcards when specifying a set name.
Example
The following command removes the set named my_set.
remove_set -name my_set