21.8.29 list_output_delays
(Ask a Question)Description
Returns details about all of the output delay constraints in the current timing constraint scenario.
list_output_delaysArguments
| Return Type | Description |
|---|---|
string | Details about all of the output delay constraints in the current timing constraint scenario. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Example
With this command we get the details about all of the output delay constraints in the current timing constraint scenario.
puts [list_output_delays]