21.8.18 list_clock_latencies
(Ask a Question)Description
Returns details about all of the clock latencies in the current timing constraint scenario.
list_clock_latenciesArguments
| Return Type | Description |
|---|---|
string | Returns details about all of the clock latencies in the current timing constraint scenario. |
Supported Families
| PolarFire® |
| PolarFire SoC |
| SmartFusion® 2 |
| IGLOO® 2 |
| RTG4™ |
Example
With this command we get the details about all of the clock latencies in the current timing constraint scenario.
puts [list_clock_latencies]