NET_PRES_CertStoreGetServerCert Function
C
bool NET_PRES_CertStoreGetServerCert(const uint8_t ** serverCertPtr, int32_t * serverCertSize, const uint8_t ** serverKeyPtr, int32_t * serverKeySize, uint8_t certIndex); Returns
true - Indicates success
false - Indicates failure
Description
Get Server Certificate and Key function This function is used by server connections to retrieve their certificate and private key. Multiple server certificates can be stored in the certificate store, for example one for a Web server and one for a mail server.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| serverCertPtr | A pointer to the server certificate |
| serverCertSize | The size of the server certificate |
| serverKeyPtr | A pointer to the server private key |
| serverKeySize | The size of the server private key |
| certIndex | Most likely '0', but this parameter is provided to select a different server certificate |