NET_PRES_SocketOptionsGet Function
C
bool NET_PRES_SocketOptionsGet(NET_PRES_SKT_HANDLE_T handle, NET_PRES_SKT_OPTION_TYPE option, void* optParam); Returns
true - Indicates success
false - Indicates failure
Description
Various options can be obtained at the socket level. This function calls directly to the transport layer's OptionGet function, if it exists.
Preconditions
A socket needs to have been opened by NET_PRES_SocketOpen.
Parameters
| Parameters | Description |
|---|---|
| handle | The socket to set options for. |
| option | The specific option to set, this is passed unaltered to the transport layer. |
| optParam | The option value, which is passed unaltered to the transport layer. |