NET_PRES_CertStoreGetCACerts Function
C
bool NET_PRES_CertStoreGetCACerts(const uint8_t ** certPtr, int32_t * certSize, uint8_t certIndex); Returns
true - Indicates success
false - Indicates failure
Description
Get CA Certificates function This function is used by client connections to retrieve the Certificate Authority certificates that are used to validate signatures on server certificates.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| certPtr | A pointer to the CA certificates |
| certSize | The size of the certificates |
| certIndex | Most likely '0', but this parameter is provided to select a different set of CA certificates |