NET_PRES_TransBind Type
C
typedef bool (* NET_PRES_TransBind)(NET_PRES_SKT_HANDLE_T handle, NET_PRES_TRANS_ADDRESS_TYPE addType, NET_PRES_SKT_PORT_T port, NET_PRES_ADDRESS * address); Returns
true - Indicates success
false - Indicates failure
Description
Transport Layer Bind Function Pointer Prototype This function is called by the presentation layer when an application wants to bind a socket.
Preconditions
A socket needs to have been opened by NET_PRES_TransOpen.
Parameters
| Parameters | Description |
|---|---|
| handle | The handle returned from NET_PRES_TransOpen. |
| addType | The type of address being used. This is passed unaltered to the transport layer. |
| port | The port to use. This is passed unaltered to the transport layer. |
| address | The address to bind to. This is passed unaltered to the transport layer. |