NET_PRES_SocketIsSecure Function
C
bool NET_PRES_SocketIsSecure(NET_PRES_SKT_HANDLE_T handle); Returns
true - If the communications is secure
false - If the communications is not secure
Description
This function returns whether or not the connection is secure. It will return true if encryption negotiation was successful .
Preconditions
A socket needs to have been opened by NET_PRES_SocketOpen.
Parameters
| Parameters | Description |
|---|---|
| handle | The presentation layer socket handle. |