NET_PRES_Initialize Function
C
SYS_MODULE_OBJ NET_PRES_Initialize(const SYS_MODULE_INDEX index, const SYS_MODULE_INIT * const init); Returns
Valid handle to the presentation instance - If successful
SYS_MODULE_OBJ_INVALID - If unsuccessful
Description
Network Presentation Layer Initialization Initializes the Network Presentation Layer sub-system with the configuration data.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| index | This is the index of the network presentation layer instance to be initialized. Since there is only one network presentation layer, this parameter is ignored. |
| init | This is a pointer to a NET_PRES_INIT_DATA structure |