NET_PRES_TransDiscard Type
C
typedef uint16_t (* NET_PRES_TransDiscard)(NET_PRES_SKT_HANDLE_T handle); Returns
The number of bytes discarded.
Description
Transport Layer Discard Function Pointer Prototype This function is called by the presentation layer when the application wants to discard the RX buffer in a socket.
Preconditions
A socket needs to have been opened by NET_PRES_TransOpen.
Parameters
| Parameters | Description |
|---|---|
| handle | The handle returned from NET_PRES_TransOpen. |