4.1.3.2.2 SNMP Trap Sources Configuration
The Trap Configuration provides SNMP trap source configurations. A Trap Destination Address is sent for the given trap source, if at least one filter matches with the included filter type. The following figure shows the SNMP trap sources configuration.
The Trap Configuration page has the following parameters:
- Name: The event for which a trap must be sent. See the preceding figure.
- Type: Include/Exclude trap for the specified event
- Subset OID: The subset OID for the entry. The value must depend on the kind of trap that is sent. For example, the ifIdex is the subset OID of linkUp and linkDown. A valid subset OID is one or more digital numbers (0–4294967295) or asterisk (*) which are separated by dots (.). The first character must not begin with asterisk (*) and the maximum OID count must not exceed 128.