1.2.2.1.1.4.70 BLE_GAP_TerminateSync
C
uint16_t BLE_GAP_TerminateSync(uint16_t syncHandle);Description
Stop reception of the periodic advertising train identified by the input "syncHandle".
Note
This API belongs to extended advertising feature. It will be disallowed if any one API that belongs to legacy advertising feature is issued before. Categories of advertising APIs and events for details of advertising APIs.
BLE_GAP_ScanInit, BLE_GAP_ExtScanInit and BLE_GAP_SyncInit are required for this API.
Parameters
| Parameter | Description |
|---|---|
| [in] syncHandle | Identity of the periodic advertising train. Range: 0x0000 to 0X0EFF |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully stop reception of the periodic advertising train. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed. |
| MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |