18.4.2.1 ADC Input Selection and Coherent Demodulation
The RDC will automatically trigger the ADC for coherent sampling. The RDCINSEL register allows the selection of the ADC instance and channel used to sample the sine and cosine outputs from the resolver.
The IMUX0 (RDCINSEL[2:0]) and IMUX1 (RDCINSEL[18:16]) bit fields can select the ADC module instances that receive the resolver output to be demodulated. For resolver outputs, the user should configure the ADC to oversample the input signals at a multiple “N” of the excitation frequency; this will be inherently true if using the excitation and trigger frequencies produced by this module due to the availability of the signal dividers using EXCFDIV bits.
If the ADC of the dsPIC33AK256MPS306 family of devices is used, then the resolver output
can be connected as input to multiple channels of the ADC. In this case, the ICHAN0
(RDCINSEL[7:3]) and ICHAN1 (RDCINSEL[23:19]) bit fields can select the ADC channels to
use for the ADC module instance selected by IMUX0 and IMUX1, respectively. If the IMUX0
and IMUX1 values do not correspond to a valid ADC module instance available in the
device, then the IMUXCFGERR (RDCSTAT[1]) bit will be set to '1'. CIC
filter channel x (x=0,1) will be fed with digital samples from the
corresponding ADC channel selected by ICHANx of the ADC module instance selected by
IMUXx. When selecting channels that are sampled sequentially on one input source or
which are sampled on different sources with some phase difference, care should be taken
to sample the inputs as close to synchronously as possible to minimize output error.