4.3.9 Alternate Working Register Arrays
Alternate Working register arrays are a subset of the Working registers (W0 through W7). Depending on the specific device, up to seven Alternate Working register arrays may be implemented. Each set implements registers W0 through W7, AccA, AccB, RCOUNT and DSP related CORCON control bits (US, SATA, SATB, SATDW, ACCSAT, RND, IF). The Alternate W registers are not memory-mapped to data memory space just like the default W array.
All W register arrays are persistent; that is, the contents of the default and Alternate W registers do not change whenever the CPU switches to another set. This saves time by reducing the amount of saving and restoring of register contents, making this very useful for time-critical applications.
Each Alternate W array is inherently assigned to a respective IPL (e.g., IPL4 is assigned to Context 4) and Interrupt Service Routine (ISR) in the application code. The Current Context Identifier (CTX[2:0]) status field is located within the Status Register (SR). Each context is associated with a specific Interrupt Priority Level (IPLV). The context is exited during execution of RETFIE instruction of the interrupt ISR.
During exception processing, the (CTX[2:0]) status field located within the Status Register (SR) is stacked. The stacked SR.CTX[2:0] represents the CPU register context in use at the time of the exception. The value is updated whenever the register context is changed, either through automatic interrupt-based hardware switching or as the result of a context change brought about by the execution of a CTXTSWP{W} instruction.
Depending on the device, different context Working register behavior can be observed with nested interrupts. Consider the example, as shown in Figure 4-3, where there are nested interrupts. In this case, the system is configured as follows.
- Timer1 interrupt with an Interrupt Priority Level (IPL) of 1. The Alternate Working Register Set 1 (CTX1) has an IPL of 1.
- ADCAN1 interrupt with an IPL of 4. The Alternate Working Register Set 4 (CTX4) has an IPL of 4.
- PWM1 interrupt with an IPL of 5. The Alternate Working Register Set 5 (CTX5) has an IPL of 5.
The application begins in the main function. At some point in time, the Timer1 interrupt flag is set and the program jumps to the Timer1 ISR. The register set switches from the default Working register set 0 to the Alternate Working register set 1, CTX1. At some point during the Timer1 ISR, the ADCAN1 conversion completes, and its interrupt flag is set. Because it has a higher IPL, the program jumps to the ADCAN1 ISR. The register set switches from the set 1, CTX1 Alternate Working register set to the Alternate Working register set 4, CTX4. At some point during the ADCAN1 ISR, the PWM1 interrupt flag is set. Because the PWM1 IPL is higher than the ADCAN1 IPL, the program jumps to the PWM1 ISR and remains in the Alternate Working register set 5 CTX5.
Once the PWM ISR execution is completed, the program jumps back to the ADCAN1 ISR using CTX4. Similarly, after the execution of the ADCAN1 ISR, the program jumps back to the Timer1 ISR using CTX1. Exceptions above IPL7 (i.e., traps) will execute in whatever register context the CPU was in prior to the trap event.