4.13 ATWILC Baremetal v3.3
The following are bug fixes and enhancements for RTP:
- Fix regression starts on release 3.0 on connection to open security AP
- Send fixed data lengths to the host for the same frame regardless of the security of the AP in the parsed option of the Monitor mode
- Fix connection issue when one ATWILC in station mode tries to connect to another ATWILC in AP mode
- Send the correct MAC address in the connect notification in case of SoftAP secured mode